Model BLM

Magnetostrictive sensor

For bypass level indicators

Selected documents
Sales contact Questions? Find a contact in your vicinity.

Applications

  • Sensor for continuous level measurement of liquids in bypass level indicators
  • Chemical and petrochemical industries, offshore
  • Shipbuilding, machine building
  • Power generating equipment, power plants
  • Pharmaceutical, food, water treatment, environmental engineering industries

Special features

  • Continuous level measurement on the outside of the bypass
  • 2-wire technology 4 ... 20 mA
  • Measured value output via digital interface and a selectable measured value as analogue signal
  • Case from stainless steel (display from glass)
  • Magnetostrictive level measuring instrument with high resolution

Description

Level sensors with a magnetostrictive, high-resolution measuring principle are used for continuous level measurement of liquids and are based on determining the position of a magnetic float following the magnetostrictive measuring principle. The sensors are mounted on the outside of a bypass level indicator.

The measuring process is triggered by a current impulse. This current produces a circular magnetic field along a wire made of magnetostrictive material, which is held under tension inside the sensor tube. At the point being measured (liquid level) there is a cylindrical float with permanent magnets acting as a position transducer, whose field lines run at right angles to the impulse magnetic field. This magnetic field of the float tensions the wire.

The superposition of these two magnetic fields triggers a mechanical wave in the wire. This is converted into an electrical signal at the end of the wire in the sensor housing by a piezoceramic pick-up.

The measured propagation delay enables the origination point of the mechanical torsional wave, and thus the float position, to be determined with high accuracy.

Magnetostrictive sensor
  • Magnetostrictive sensor
Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.