Download

Pressure controllers

Models: CPC6050, CPC4000
Instrument Software V2.40.0

The software upgrade installer for the CPC4000 or CPC6050 is used to upgrade a new CPC4000 or CPC6050's software to the most recent version. (Not for auto ranging single output CPC6050s)

ZIP (3.6 MB)
Instructions (3.6 MB)
Models: CPC6050
Auto Ranging Single Output V2.40.0

The software upgrade installer for the Auto Ranging Single Output Version of the CPC6050 ONLY. It is used to upgrade an Auto Ranging Single Output CPC6050 software to the most recent version. (Not for dual channel CPC6050s. To determine if your CPC6050 is a Single Output version view the info screen on your CPC6050, it will be designated as "Model: CPC6050 (Single Output)".

ZIP (1.9 MB)
Models: CPC8000
Instrument Software V1.47.0

The software upgrade installer for the CPC8000 is used to upgrade a new CPC8000's software to the most recent version.

ZIP (2.6 MB)
CPC6000 Instrument Software V2.70.0

The software upgrade installer for the CPC6000 is used to upgrade a new CPC6000’s software to the most recent version. The Download includes the latest version, and the older version 1.70. Your CPC6000 will automatically detect and install the correct version.

ZIP (1.5 MB)
CPC3000 Instrument Software V2.14.0

The CPC3000 software upgrade installer is used to upgrade a new CPC3000’s software to the most recent version.

ZIP (1.1 MB)
Models: CPA8001
Instrument Software V1.40.0

The software upgrade installer for the CPA8001 is used to upgrade a CPA8001's software to the most recent version.

ZIP (2.7 MB)
Models: CPC8000-H
Instrument Software V1.47.0

The software upgrade installer for the CPC8000-H is used to upgrade a new CPC8000-H's software to the most recent version.

ZIP (2.6 MB)
Models: CPB3800, CPB5600DP, CPB5800, CPB6000DP, CPB8000, CPD8000, CPG2500 Barometer, CPG500, CPH6300, CPH65I0, CPT6010, CPT6010 Barometer, CPT6100 Barometer, CPT6600, CPU6000-W, CPU6000-S, CPU6000-M, CPU5000, CTI5000, CTR1000, Pascal 100, Pascal ET, WIKA-Cal, CPG2300, CPB5000, CPC8000-H, CPG2500, CPC2000, CPC8000, CPH62I0, CPT2500, CPC7000, CPB5000HP, CPT6100, CPT6180, CPH6000, CPH6200, CPH6400, CPG-KITP, CPG-KITH, CPH7000
WIKA-CAL V1.0.78

Calibration software; System requirements Windows® 2000, XP, Vista, 7

ZIP (5.2 MB)
Instructions (15.3 MB)
Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.