Contact pressure gauges

WIKA contact pressure gauges: Switching and indicating with a single instrument

Wherever the process pressure has to be indicated locally and, at the same time, limit values must be monitored, contact pressure gauges find their application. The switch contacts make or break the circuit dependent upon the pointer position of the indicating measuring instrument. If the reading is significantly above or below a set value, they trigger an alarm, hence also the term “alarm contact”. Contact pressure gauges are also suitable for starting, stopping or switching processes.

Calibration services

Entrust the calibration and maintenance of your measuring instruments to a competent partner.

Details
Sales contact Questions? Find a contact in your vicinity.


FAQ

What is meant by switching function?

Under switching function, we mean the opening or closing of an electrical circuit. Normally-closed contacts (NC, denoted by a 2) interrupt a circuit on rising pressure (clockwise); normally-open contacts (NO, denoted by a 1) close a circuit on rising pressure (cloc ... More

What is the function of a four or five-way valve block?

These pressure-equalising valves (with integrated shut-off, purge and vent valves) enable the pressure gauge to be vented on one or both sides and the supply line to be purged.

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.