Temperature switches are used in a variety of industrial and technical processes. If a preset temperature is reached, then the temperature switch opens or closes a corresponding switch contact. Depending on the requirements, mechanical or electronic switches can be used. In WIKA's broad product range, you will find the right temperature switch for every application.

Sales contact Questions? Find a contact in your vicinity.


FAQ

How does a resistance thermometer work?

The electrical resistance of a resistance thermometer's sensor changes with the temperature. As the resistance of measuring resistors to EN 60751 (2009-05) increases with rising temperature, we refer to it as PTC ... More

Why should Pt100 measuring circuits with reduced tolerance class A or AA per DIN EN 60751 be used in at least a 3- or 4-wire connection?

The 2-wire connection is not permissible for classes A and AA per DIN EN 60751 since here the internal lead resistance of the wires is added to the measured value. This will usually exceed the specified tolerance for the temperature sensor. A measurement of the cab ... More

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.