Thermometers with switch contacts

Wherever the process temperature has to be indicated locally and, at the same time, limit values must be monitored, thermometers with switch contacts find their application. The switch contacts make or break the circuit dependent upon the pointer position of the indicating measuring instrument. If the reading is significantly above or below a set value, they trigger an alarm, hence also the term “alarm contact”. The instruments are also suitable for starting, stopping or switching processes.

Sales contact Questions? Find a contact in your vicinity.


FAQ

What is a sliding contact (model 811)?

The sliding contact is a mechanical physical contact for switching loads of up to 10W 18VA.

What is meant by switching function?

Under switching function, we mean the opening or closing of an electrical circuit. Normally-closed contacts interrupt a circuit on rising temperature (clockwise); normally-open contacts close a circuit on rising temperature (clockwise).

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.