Model GDS-MV

Gas density switch

For medium voltage

Selected documents
Sales contact Questions? Find a contact in your vicinity.

Applications

  • Medium-voltage equipment
  • Gas density monitoring of closed SF6 gas tanks
  • Ring main units (RMU)

Special features

  • Independent of atmospheric pressure and altitude
  • No recalibration required

Description

Gas density is a crucial operating parameter for medium-voltage systems. If the required gas density is not present, safe operation of the plant cannot be guaranteed. The gas density measuring instruments from WIKA warn reliably against dangerously low gas quantities, even under extreme environmental conditions. Electrical switch contacts warn the plant manager if the gas density, on account of a leak, drops below a specified value.

Numerous fields of application
The WIKA gas density switches are hermetically sealed and temperature compensated. Measured value fluctuations and erroneous alarms caused by changes in either ambient temperature or air pressure are therefore prevented.

Gas density switch
  • Gas density switch
Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.