Contact pressure gauges

WIKA contact pressure gauges: Switching and indicating with a single instrument

Wherever the process pressure has to be indicated locally and, at the same time, limit values must be monitored, contact pressure gauges find their application. The switch contacts make or break the circuit dependent upon the pointer position of the indicating measuring instrument. If the reading is significantly above or below a set value, they trigger an alarm, hence also the term “alarm contact”. Contact pressure gauges are also suitable for starting, stopping or switching processes.

Calibration services

Entrust the calibration and maintenance of your measuring instruments to a competent partner.

Details
Sales contact Questions? Find a contact in your vicinity.


FAQ

What is an electronic contact (model 830.E)?

Electronic contacts are fitted with non-contact slot sensors. They are especially suitable for oil-filled gauges and should be preferred for low voltages and small DC loads, such as for the signal input for a PLC (programmable logic controller).

What is the function of a three-way valve block?

With upstream pressure equalising valves it is possible to achieve uniform pressure loading from the plus and minus side, to avoid single-sided overpressure loading during both start-up and operation, and also to enable zero point checks during operation.

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.