Submersible pressure sensors

The submersible pressure sensor, sometimes also referred to as a level probe, is a special type of pressure sensor for hydrostatic level measurement in tanks, wells, shafts and bore holes. For this, the submersible pressure sensor is submerged directly in the liquid to be measured, and positioned as close as possible to the bottom. There, the submersible pressure sensor measures the hydrostatic pressure, which enables a direct conclusion regarding the current level, i.e. the height of the liquid column above it.

Sales contact Questions? Find a contact in your vicinity.


FAQ

Where is the submersible pressure sensor installed?

The submersible pressure sensor is installed at the lowest measuring point.

Can the connector be altered?

The electrical connection cannot be altered.

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.